Technical FAQs

Ask a Question

Is it possible to upgrade a 140CPU43412 [non A] from Concept to Unity Pro?

No. Only the 140CPU43412A with a PV:04 or greater can be upgraded to support Unity Pro. If the (A) version is PV16 or greater you need to use the RoHS firmware.


Was this helpful?
What can we do to improve the information ?