Technical FAQs

Ask a Question

What terminal connector would be used with the Sy/Max 16 point input and output modules?

The Sy/Max 16 point input and output modules terminal blocks are the same part number, 8030-CBP-116. These terminal connectors are supplied with the module.

Was this helpful?
What can we do to improve the information ?