Technical FAQs

Ask a Question

What is the Maximum amount of consecutive bits/words the M340 Read_Var function can handle per operation?

The Modicon M340 PLC READ_VAR function can read up to 2,000 consecutive
bits or 125 words in a remote device per read operation.

Was this helpful?
What can we do to improve the information ?