Technical FAQs

Ask a Question

What is the maximum number of available words allowed on the Unity RIO Network ? (CRP93x 00/CRA93x 00)

The Unity RIO Network allows 64 input words and 64 output words per drop. There can be a maximum of 31 remote drops.


Legacy KB System (APS) Data: RESL210941 V1.0, Originally authored by DaSo on 03/13/2013, Last Edited by DaSo on 03/13/2013
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?