Technical FAQs

Ask a Question

Is there a Telefast solution with premade cables for the 16 channel M340 discrete I/O modules?

There is no Telefast solution with premade cables for the 16-channel M340 discrete I/O modules.
However, the higher density discrete I/O modules (32 and 64 channel) do have a Telefast solution.


Legacy KB System (APS) Data: RESL210939 V1.0, Originally authored by DaSo on 03/13/2013, Last Edited by DaSo on 03/13/2013
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?