Technical FAQs

Ask a Question

What is the maximum number of available words on the Unity Ethernet RIO Network?

Each ERIO drop can support 400 input words & 400 output words. A total of 32 drops are allowed on the ERIO Network.
Total input words per ERIO Network is 16K. Total output words per ERIO Network is 12K.

Was this helpful?
What can we do to improve the information ?