Technical FAQs

Ask a Question

What is the Advantys FTXES01?

The Advantys FTXES01 is the Lite version of the Advantys configuration software and it is only for the OTB with the Twido IO and does not require authorization. For the Advantys STB hardware, you will need to install the full package and authorize it part number STBSPU1000.


Legacy KB System (APS) Data: RESL210932 V1.0, Originally authored by DiSa on 03/12/2013, Last Edited by DiSa on 03/12/2013
Related ranges: Modicon OTB
Was this helpful?
What can we do to improve the information ?