Technical FAQs

Ask a Question

Is there a wiring arm cable combination for the BMXAMM0600?

Yes, the BMXFTW301S or the BMXFTW501S is available. Each cable has one 20-way connector on one end and a pigtail of wires on the other. The difference between the two is the length, one is 3 m and the other 5m.


Legacy KB System (APS) Data: RESL210931 V1.0, Originally authored by DaSo on 03/12/2013, Last Edited by DaSo on 03/12/2013
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?