Technical FAQs

Ask a Question

What is the replacement for the FTXCY1212 Y-connector used to connect 2 M12-type connectors to an M12 connector ?

The FTXCY1212 is obsolete and there is no replacement. Contact the vendor, Murrelektronik, from whom Schneider Electric purchased these connectors. Their website is www.murrelektronik.com. Refer to the 'Field Active' solutions product line.


Legacy KB System (APS) Data: RESL210924 V1.0, Originally authored by DaSo on 03/09/2013, Last Edited by DaSo on 03/09/2013
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?