Technical FAQs

Ask a Question

Which Quantum PLCs have the Factory Mutual (FM) Class 1 Div. 2 rating?

All Quantum CPUs are FM Class 1 Div 2 approved.
140CPU11302
140CPU11303
140CPU43412A
140CPU53414A
140CPU53414B
140CPU65150
140CPU65160
140CPU652 60
140CPU67160
140CPU67260
140CPU67261
140CPU65160S (SIL 3 / ATEX Zone 2/22) This CPU meets and exceeds the FM Class 1 Div. 2 rating
140CPU67160S (SIL 3 / ATEX Zone 2/22) This CPU meets and exceeds the FM Class 1 Div. 2 rating

..


Legacy KB System (APS) Data: RESL210922 V1.0, Originally authored by DaSo on 03/09/2013, Last Edited by DaSo on 03/09/2013
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?