Technical FAQs

Ask a Question

What options are available for connecting to an Advantys STBNIP2212 or STBNIP2311 when launching the configuration software from within Unity Pro I/O scanner screen ?

When launching the Advantys Configuration software from within the Unity Pro I/O scanner configuration screen, the only option for connecting is via the configured IP in the I/O scanner table. Connecting serially is not an option.


Legacy KB System (APS) Data: RESL210892 V1.0, Originally authored by DaSo on 03/06/2013, Last Edited by DaSo on 03/06/2013
Related ranges: Modicon STB
Was this helpful?
What can we do to improve the information ?