Technical FAQs

Ask a Question

What is error number 19002 on a Sy/Max PLC?

An error number 19002 is a slot error. 190EE where EE points to the slot number experiencing the error so 19002 points to slot number 2. POSSIBLE CAUSES below:
1) Improper rack addressing in which remote drops are assigned to a slot which contains a LI or LTI card.
2) Improper seating of module in rack, edge connector of module may be damaged or the rack or slot has been damaged.

Legacy KB System (APS) Data: RESL210813 V1.0, Originally authored by DiSa on 02/28/2013, Last Edited by DiSa on 02/28/2013
Related ranges: Sy/Max
Was this helpful?
What can we do to improve the information ?