Technical FAQs

Ask a Question

What are the full dimensions of the Magelis Touch Screen XBTGT7340?

Below are the full dimensions for the XBTGT7x series.




Legacy KB System (APS) Data: RESL210802 V1.0, Originally authored by WiAl on 02/28/2013, Last Edited by WiAl on 02/28/2013
Related ranges: Magelis XBT GT, Vijeo Designer
Was this helpful?
What can we do to improve the information ?