Technical FAQs

Ask a Question

Can you update the M340 CPU firmware using the BMXNOE0100 Ethernet connection?

No. You must be connected directly to the M340 CPU using USB, Ethernet or Modbus.


Legacy KB System (APS) Data: RESL210795 V1.0, Originally authored by DaSo on 02/27/2013, Last Edited by DaSo on 02/27/2013
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?