Technical FAQs

Ask a Question

Is it possible to update the firmware of the BMXNOE 01xx module through the NOE's native Ethernet port?

Yes. In fact a direct connection to the BMXNOE01xx is the only approved connection method for performing the firmware upgrade.


Legacy KB System (APS) Data: RESL210792 V1.0, Originally authored by DaSo on 02/27/2013, Last Edited by DaSo on 02/27/2013
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?