Technical FAQs

Ask a Question

Why is the 140CPS12420 not compatible with the 140CPS12400 when used in a redundant configuration ?

The two power supplies cannot share the output current normally due to the difference of their internal parameters. The internal current APS_SENSORS do not have the same gains. If the two power supplies operate in parallel, this will cause one power supply to not operate normally with its PWR OK LED off.


Legacy KB System (APS) Data: RESL210789 V1.0, Originally authored by DaSo on 02/27/2013, Last Edited by DaSo on 02/27/2013
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?