Technical FAQs

Ask a Question

What constitues an M340 warm start?

When a power outage occurs on an M340 PLC and the project that has been backed up is the same
as the project in on the SD card, a warm start occurs.


Legacy KB System (APS) Data: RESL210766 V1.0, Originally authored by DaSo on 02/26/2013, Last Edited by DaSo on 02/26/2013
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?