Technical FAQs

Ask a Question

What's the part number of the Fiber Optic Cable that comes with the 140CHS21000 Hot Standby Kit?

The part number of the Fiber Optic Cable that comes with the 140CHS21000 Hot Standby Kit is 990XCA65609.


Legacy KB System (APS) Data: RESL210722 V1.0, Originally authored by RoAl on 02/21/2013, Last Edited by RoAl on 02/21/2013
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?