Technical FAQs

Ask a Question

What is the maximum traffic capacity of a 140NOC78100 ?

The maximum traffic capacity of a 140NOC78100 is (1300 pps (IP routing traffic) + 4500 pps (I/O communication)) OR 5000 pps IP routing traffic.


Was this helpful?
What can we do to improve the information ?