Technical FAQs

Ask a Question

How do I create network names in ProWORX NxT software?

Goals and Symptoms

To create network names in ProWORX NxT.

Causes and Fixes

To create network names in ProWORX NxT.

Attachments

Make sure that your cursor is on a blank spot in the network, or a short, not an element. Go to Display and Documentation Editor to open the Documentation Editor for the network. Enter the Network name in the Page Title box and click the OK button.
(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/626f18e9fcef04f6c1257b170016152c/fl_block_5/67.3CE8?OpenElement&FieldElemFormat=gif)

The network page title will now appear on the logic screen.

(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/626f18e9fcef04f6c1257b170016152c/fl_block_5/146.2802?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL210694 V1.0, Originally authored by RoAl on 02/19/2013, Last Edited by RoAl on 02/19/2013
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?