Technical FAQs

Ask a Question

Why can't I get my Sy/Max 8020 SCP401 processor to work with floating point math?

The Sy/Max 8020 SCP401 processor does not support floating point math. The 8020 SCP423, SCP424, and SCP444 do support floating point math.


Note: The Sy/Maxproduct line was obsoleted in 2013
Was this helpful?
What can we do to improve the information ?