Technical FAQs

Ask a Question

Does Unity Pro support the 140CRP81100 Quantum Profibus module?

No, Unity Pro does not support the 140CRP81100 Quantum Profibus module. When you import a program into Unity Pro, Unity Pro will change the 140CRP81100 to a Prosoft PTQ-PDPMV1 module. For this you will need to get the Prosoft module and below is the link for information on the card and ordering.

http://www.prosoft-technology.com/content/view/full/6999
text

Was this helpful?
What can we do to improve the information ?