Technical FAQs

Ask a Question

Why does the PID_INT output oscillate between Out_Max Out_Min?

The output oscillates when the PID_INT block is programmed in the MAST Task. The PID_INT block must be placed in a Periodic Task.


Legacy KB System (APS) Data: RESL210505 V1.0, Originally authored by DaSo on 02/01/2013, Last Edited by DaSo on 02/01/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?