Technical FAQs

Ask a Question

What is the replacement part number for the Quantum power supply field power connector?

All of the Quantum power supplies use the IP20 field power connector part number 140XTS00500, all of the other connector part numbers are obsolete.


Legacy KB System (APS) Data: RESL210492 V1.0, Originally authored by DiSa on 01/31/2013, Last Edited by DiSa on 01/31/2013
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?