Technical FAQs

Ask a Question

What causes the error 'Requested programmer connect mode is not available. Do you wish to use monitor mode instead? PLC is already reserved by entity: EMPTY' when trying to connect to an M340 with Unity Pro.

This was once a recurring issue that was addressed with the V2.1 firmware release. Make sure that the M340 is at V2.1 firmware or higher.


Legacy KB System (APS) Data: RESL210458 V1.0, Originally authored by DaSo on 03/07/2013, Last Edited by DaSo on 03/07/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?