Technical FAQs

Ask a Question

Does the M340 have an internal temperature value (%SW, system word) that is available to the program?

No, there is no %SW or system word which contains the internal temperature value of the M340 CPU.


Legacy KB System (APS) Data: RESL210403 V1.0, Originally authored by DaSo on 01/23/2013, Last Edited by DaSo on 01/23/2013
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?