Technical FAQs

Ask a Question

Where can I get the Vijeo Designer Runtime install files?

The VJD Runtime install files are provided with the VJD disk under \\DVD\Tools\VJD Runtime Windows
You need to enter the product reference and serial number during the installation and VJD Runtime requires authorization. Otherwise VJD Runtime will run in DEMO mode for 21 days.

The catalog number to purchase VJD Runtime on a IPC is VJDSNRTMPC.


Legacy KB System (APS) Data: RESL210166 V1.0, Originally authored by MiMe on 12/28/2012, Last Edited by MiMe on 12/28/2012
Related ranges: Vijeo Designer
Was this helpful?
What can we do to improve the information ?