Technical FAQs

Ask a Question

Quantum 140NOE77100 crashed and unable to recover from it.


1) Replacement is 140NOE77101.
2) Can be replaced without Configuration change while the controller is running. (IO Mapping mismatch will be present)
3) IO Mapping configuration update will required a complete download.


Legacy KB System (APS) Data: RESL210165 V1.0, Originally authored by MiMe on 12/28/2012, Last Edited by MiMe on 12/28/2012
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?