Technical FAQs

Ask a Question

What is the the number of candela per square meter for the Magelis XBTGTO?


HMIGTO 3.5" = 450
HMIGTO 5.7" = 500
HMIGTO 7" = 350
HMIGTO 7.5" = 400
HMIGTO 10.4" = 450
HMIGTO 12.1" = 450


Legacy KB System (APS) Data: RESL210164 V1.0, Originally authored by MiMe on 12/28/2012, Last Edited by MiMe on 12/28/2012
Related ranges: Vijeo Designer
Was this helpful?
What can we do to improve the information ?