Technical FAQs

Ask a Question

Is there a replacement for the AS-B875-002 800 IO series slot mount card?

The AS-B875-002 is obsolete but has been replaced by the AS-B875-111. The AS-B875-111 uses a different terminal connector AS-8535-000 and required rewiring the card for the new connector.


Legacy KB System (APS) Data: RESL210162 V1.0, Originally authored by MiMe on 12/28/2012, Last Edited by MiMe on 12/28/2012
Related ranges: Modicon 1/2/3/4/5/8/984s
Was this helpful?
What can we do to improve the information ?