Technical FAQs

Ask a Question

What is the maximum Elevation or Altitude for the M340 PLC.

Goals and Symptoms

What is the maximum Elevation or Altitude for the M340 PLC.

Causes and Fixes

M340 Operating Conditions and Environment Related Recommendations:
Max. Altitude 4,000 meters (13,124 feet)

Was this helpful?
What can we do to improve the information ?