Technical FAQs

Ask a Question

What are the specifications for the TELEFAST ABFH20H200 cable?

Goals and Symptoms

The purpose of this resolution is to provide the specifications of the TELEFAST Cable bearing part number ABFH20H2000

Facts and Changes

TELEFAST cable bearing part number ABFH20H2000 (20 m cable) is obsolete and cannot be ordered from Schneider anymore. The only available cable is ABFH20H200 which is 2m in length.

Causes and Fixes

Since there is no direct replacement, the manufacturer's catalog numbers for the cable and connector are provided in this resolution. Hence this shall serve as an alternative solution.
Rolled Ribbon Cable - 28 AWG gauge (0,08 mm^2 cross-section) Catalog number : ABFC20R200
20 way HE Connector - Catalog number ABC6HE20F

The cable is a one-one straight cable.


Legacy KB System (APS) Data: RESL210031 V1.0, Originally authored by TVe on 12/14/2012, Last Edited by TVe on 12/14/2012
Related ranges: Modicon ABE7
Was this helpful?
What can we do to improve the information ?