Technical FAQs

Ask a Question

Can I use the 52-0402-000 Tap Port Terminator as a Trunk Terminator?

No. The Modicon 52-0422-000 Trunk Terminator is a precision 75 OHM, 1% tolerance, 14dB terminating resistor specifically designed for trunk termination. Do not use the 52-0402-000 Tap Port Terminator to terminate the trunk cable.

 
Was this helpful?
What can we do to improve the information ?