Technical FAQs

Ask a Question

In Vijeo Designer 6.0, why is the "included editor project" is missing?

To enable the "include editor project", you need to go to the Data Locations of the Target Property. Change the "Data Files / Forms" from "Main Drive" to either "Secondary Drive" or "Optional Drive".

Was this helpful?
What can we do to improve the information ?