Technical FAQs

Ask a Question

Is there a 28 point screw terminal connector for use with M340 I/O modules, similiar to the BMXFTB2820, which is a spring type terminal connector?

Yes, the 28 point screw terminal connector is BMXFTB2800.


Legacy KB System (APS) Data: RESL209908 V1.0, Originally authored by DaSo on 12/07/2012, Last Edited by DaSo on 12/07/2012
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?