Technical FAQs

Ask a Question

What are the specifications and wiring diagram for the Modicon M340 BMXDAI1604 Module?

See attached for the Modicon M340 BMXDAI1604 specifications and wiring diagram.
BMXDAI1604.pdf


Legacy KB System (APS) Data: RESL209904 V1.0, Originally authored by DiSa on 03/02/2013, Last Edited by DiSa on 03/02/2013
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?