Technical FAQs

Ask a Question

Is the best way to flash the OS of a Unity 140CPU65150 to use USB or MB+?

USB is not supported for flashing the OS with the OS Loader. Only Modbus Plus or Modbus can be used. The CoPro must be flashed using Ethernet.


Legacy KB System (APS) Data: RESL209903 V1.0, Originally authored by DaSo on 12/08/2012, Last Edited by DaSo on 12/08/2012
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?