Technical FAQs

Ask a Question

What is the part number for a screen protector to either the XBTGT7340 or HMIGTW7353.

Goals and Symptoms

What is the part number for a screen protector to either the XBTGT7340 or HMIGTW7353.

Causes and Fixes

MPCYK50SPSKIT is the part number for the screen protecter to both XBTGT7340 and HMIGTW7353.


Legacy KB System (APS) Data: RESL209831 V1.0, Originally authored by WiAl on 12/03/2012, Last Edited by WiAl on 12/03/2012
Related ranges: Magelis XBT GT
Was this helpful?
What can we do to improve the information ?