Technical FAQs

Ask a Question

What is the pin assignment of CAN bus cable VW3M3805R010 ? (9 pin D-sub to RJ45)

Goals and Symptoms

The pin assignment of CAN bus cable VWM3805R010 which has a 9 pin D-Sub to RJ45 is shown below.
This cable may be used to connect the CAN bus from a Modicon M238 to Lexium32 or Altivar 61/71









Note: There is a 120 ohm terminating resistor connected between CAN_L and CAN_H on cable VWM3805R010
 

Causes and Fixes

NA


Legacy KB System (APS) Data: RESL209784 V1.0, Originally authored by TVe on 11/28/2012, Last Edited by TVe on 11/28/2012
Related ranges: Lexium 32
Was this helpful?
What can we do to improve the information ?