Technical FAQs

Ask a Question

Why Unity Loader does not run in the language chosen during installation?

When Unity Loader is first launched after being installed, by default it will run using the language of the Operating system of the PC on which it is installed.
If this language is not suitable, to select the language needed (see attached the image below) :
- select the Options Tab,
- select the Language in the scroll list
- close and relaunch Unity Loader.
It will then run in the language selected.

screen_Unity_loader.zipscreen_Unity_loader.zip


Legacy KB System (APS) Data: RESL209582 V1.0, Originally authored by ChAn on 11/06/2012, Last Edited by ChAn on 11/06/2012
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?