Technical FAQs

Ask a Question

What does the "H" at the end of the Modicon M340 part number mean?

The "H" at the end of the Modicon M340 part number stands for the "Ruggedized" version. This version allows the M340 to be used in more severe environments because of the protective coating on all their circuit boards and has an extended temperature range from - 25C to + 70C.

Legacy KB System (APS) Data: RESL209489 V1.0, Originally authored by DiSa on 10/25/2012, Last Edited by DiSa on 10/25/2012
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?