Technical FAQs

Ask a Question

How do I map six NOE771xx modules in a Hot Standby system using Concept 2.5 software?

The proper way to I/O map six NOE modules in a Concept 2.5 Hot Standby configuration is to first enter and configure all of the NOE's . Then enter the CRP's in the I/O Map. If this is not done in the order described, the NOE may not power up correctly in the rack. The only CPU's that will support 6 NOE's are the 140CPUx341x and the 140CPU42402.


Legacy KB System (APS) Data: RESL2093 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?