Technical FAQs

Ask a Question

Can multiple position registers of Lexium 32 be assigned to a single output?

This FAQ is regarding the four position registers of Lexium 32.
When setting the position registers each register must be assigned to a separate output.
It is not possible with the current firmware to assign more than one register to a single output.
Therefore to use all four position registers, and each of them being assigned to their own output, it would require the use of the I/O expansion module which is only available for use with Lexium 32M.


Legacy KB System (APS) Data: RESL209150 V1.0, Originally authored by TVe on 09/20/2012, Last Edited by TVe on 09/20/2012
Related ranges: Lexium 32
Was this helpful?
What can we do to improve the information ?