Technical FAQs

Ask a Question

Will the digital outputs in a Lexium 32 turn on when configured for Motor Standstill condition even if the drive is not Enabled?

Goals and Symptoms

The objective of this resolution is to inform the user about certain operational aspects of the outputs on a Lexium 32 drive.

Facts and Changes


Please refer to the Lexium 32C/A/M user manual for the different functions that the outputs can be configured for.

Causes and Fixes

1. If the output is configured for a Motor Standstill condition, will the output turn on, even if the drive is disabled?
Yes, the output when configured for Motor Standstill condition will turn, regardless of whether the drive is enabled or disabled.

2. Can the drive's output be configured to turn on when the motor is turning, regardless of speed or any other criteria?
No the output cannot be configured to turn just to indicate the motor is moving.
 


Legacy KB System (APS) Data: RESL209070 V1.0, Originally authored by TVe on 09/12/2012, Last Edited by TVe on 09/12/2012
Related ranges: Lexium 32
Was this helpful?
What can we do to improve the information ?