Technical FAQs

Ask a Question

Does SoMove version 1.3.5.0 support object monitoring?

SoMove software users who have had prior experience with Lexium CT software may notice that the object monitoring function found in Lexium CT can not be found in SoMove.
This is due to the fact that the current version 1.3.5.0 of SoMove does not support object monitoring as found in Lexium CT.

Note: There are plans to implement the object monitoring feature in a later revision of SoMove.


Legacy KB System (APS) Data: RESL209021 V1.0, Originally authored by TVe on 09/06/2012, Last Edited by TVe on 09/06/2012
Related ranges: SoMove
Was this helpful?
What can we do to improve the information ?