Technical FAQs

Ask a Question

Is the STBNIP2212 Ethernet Full Duplex ?

The STBNIP2212 Ethernet NIM is a 10Mbit/s, half duplex device. The newer Ethernet NIM, the STBNIP2311, is a 10/100 Mbit/s, half or full duplex device.


Legacy KB System (APS) Data: RESL208938 V1.0, Originally authored by DaSo on 08/23/2012, Last Edited by DaSo on 08/23/2012
Related ranges: Modicon STB
Was this helpful?
What can we do to improve the information ?