Technical FAQs

Ask a Question

What is the maximum bus length for a CANopen network where TWDNCO1M is the CANopen master module?

The maximum bus length for a CANopen network where TWDNCO1M is the master module (on a single CANopen segment, without repeater) is 500 m (1,640 ft) at 125 kbps.
Note:
The current Twido Programmable Controller Catalog published on October 2012 lists the maximum bus length as "30 m to 120 m". Those values are not correct, they are a misprint and will be corrected in the next catalog.


Legacy KB System (APS) Data: RESL208713 V1.0, Originally authored by TVe on 07/25/2012, Last Edited by TVe on 07/25/2012
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?