Technical FAQs

Ask a Question

Will open inputs on the 170ARM37030 cause a fault (I/O Error)?

No, open inputs on the ARM37030 will not cause a fault. The inputs are not monitored for an open circuit. The Momentum IO Base User Guide incorrectly states that an I/O Error signal will be activated as long as the inputs are open.

Was this helpful?
What can we do to improve the information ?