Technical FAQs

Ask a Question

What version of Windows 7 is supported by ProWORX 32

Goals and Symptoms

What version of Windows 7 is supported by ProWORX 32

Facts and Changes

ProWORX 32 version 2.1, SP2

Causes and Fixes


ProWORX 32 version 2.1, SP2 is qualified to be installed on Windows 7 Professional (32 Bit and 64 Bit) and Windows 7 Ultimate (32 Bit and 64 Bit). 'ProWORX 32' has not been qualified to work with Windows 7 Home Premium. Qualification testing has only been performed on Windows 7 Professional and Windows 7 Ultimate.


Attempts to install 'ProWORX 32 version 2.1' on Windows 7 Home Premium (32 Bit and 64 Bit) will return the following 'Self-registration Error' stating 'This version of is not compatible with the version of Windows you're running'.

Was this helpful?
What can we do to improve the information ?