Technical FAQs

Ask a Question

What can caused a "Runtime Error 429, Active X component cannot create object" when launching the Vijeo Historian 4.3 Excel client? "

Microsoft Office 2010 must be installed as a 32-bit version and not the 64-bit to be backwards compatible with the Excel Client.


Legacy KB System (APS) Data: RESL208023 V1.0, Originally authored by MiMe on 05/01/2012, Last Edited by MiMe on 05/01/2012
Related ranges: Monitor Pro
Was this helpful?
What can we do to improve the information ?